Configuration of OPC HDA Collector-Specific Fields
Enter the value for the OPC HDA Collector-specific field parameters through the OPC HDA Collector Maintenance - Configuration tab of the Historian Administrator.
Descriptions for collector-specific fields are listed in the following table.
Note: If the following fields are updated, then the collector must be restarted for the update to take effect.
Field | Description |
---|---|
OPC HDA Server | This field represents the OPC HDA Server ProgID to which the collector connects. By default, it points to the OPC HDA server ProgID that was entered at the time of installation. |
Recovery Time (in hours) | This field is used by the collector on start up to get the specified number of hours of data of the added tags from the OPC HDA server, and then pushes the data to Historian.
|