Backing up Archives Using Volume Shadow Copy Service
VSS provides fast volume capture of the state of a disk which is called a snapshot or shadow copy. When the snapshot is taken, disk writes are suspended for a brief period of time, typically on the order of milliseconds. After the snapshot, disk writes can resume, but the original state of the files are maintained by a difference file. The different file allows the state of the original file at the time of the snapshot to be reconstructed. This behavior allows files to be backed up while new data is being written to files.
The Volume Shadow Copy feature is provided by Windows Operating System, and the instructions to use backup and restore vary depending on the backup application that is used in the Windows operating system.
- Windows 7
- Windows 8.1
- Windows 10
- Windows Server 2008 R2
- Windows Server 2012 R2 64-bit
The Backup and Restore Center in Windows Server 2008 32-bit and 64-bit do not allow you to backup selected files or folders. However, you can do volume backups. The features available in the Backup and Restore Center depend on the Windows editions. If you need additional assistance with using Windows Server Backup Wizard, refer to Microsoft's website at: http://technet.microsoft.com/en-us/library/cc753528.aspx
In addition to using the Backup and Restore wizard, you can also use the command line utilities:- Refer to How to use command line parameters with the Ntbackup command: http://support.microsoft.com/kb/814583
- Refer to How to use command line parameters with the Wbadmin command: http://technet.microsoft.com/en-us/library/cc754015(WS.10).aspx
- If you need additional assistance about using Windows Server Backup Wizard, refer to Microsoft's website at: http://technet.microsoft.com/en-us/library/cc753528.aspx