ihuGetEnumeratedSets

Prototype

Use the ihuGetEnumeratedSets function to retrieve all the enumerated sets that match the setname mask criteria. To retrieve all sets, pass * as the mask.

ihuErrorCode IHUAPI ihuGetEnumeratedSets (
in long serverhandle,
in MSO Char *EnumeratedSetMask,
out long *numberofrecords,
out ihuEnumeratedSetRecordSet
*EnumeratedSetRecordSet  )

Remarks

The ihuGetEnumeratedSets function returns the number of enumerated set records, plus the enumerated sets.

Returns

The ihuGetEnumeratedSets function returns ihuSTATUS_OK on success, or errors if invalid input parameters are found or if out-of-memory issues occur during dynamic memory allocation.