Starting an iFIX Collector
The preferred way to start an iFIX Collector is to add the collector to the iFIX System Configuration Utility (SCU) startup list. The collector then starts automatically whenever you start iFIX
To add the collector to the SCU list, open the Task Configuration dialog box in the SCU and enter ihFixCollector.exe in the Filename field and runasdos
in the Command Line field.
You can also start an iFIX Collector as a console application, using the Start button on the Windows toolbar and the Historian 6.0 Program Startup Group.
To shutdown an iFIX Collector running as a console application, type "s" in the console window and press Enter.
If iFIX database contains a large number of blocks, you can use the Delay Collection at Startup property of the collector to give the I/O driver a chance to read data into the blocks.