Summary of OPC Collector Features

Important: You do not have the latest version of Historian! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Historian product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GE Digital Sales Support. For the most up-to-date documentation, go here.

The following table outlines the features of the OPC Collector.

Feature Capability
Browse Source For Tags Yes (on OPC Servers that support browsing)
Browse Source For Tag Attribute Yes
Polled Collection Yes
Minimum Poll Interval 100 ms
Unsolicited Collection Yes (OPC 2.0 Only)

If you are using an OPC Collector with unsolicited data collection and have collector compression disabled, all new values should produce an exception. When the OPC Collector is doing unsolicited collection, the deadband percentage is determined by the collector deadband percent. You can only configure the collector deadband percent by enabling compression.

Timestamp Resolution Yes
Accept Device Timestamps Yes
Floating Point Data Yes
Integer Data Yes
String Data Yes
Binary Data Yes
Python Expression Tags Yes