Summary of File Collector Features

Important: You do not have the latest version of Historian! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Historian product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GE Digital Sales Support. For the most up-to-date documentation, go here.

The following table outlines the features of the File Collector.

Feature Capacity
Browse Source For Tags No
Browse Source For Tag Attributes No
Polled Collection No
Maximum Poll Rate N/A
Unsolicited Collection No
Time Stamp Resolution 1 ms
Accept Device Timestamps Yes
Floating Point Data Yes
Integer Data Yes
String Data Yes
Binary Data No
Import CSV Files Yes
Import XML Files Yes
Import multiple files with various extensions Yes
Collector compression No
Reads data, tags and messages Yes
Start/stop collection from Historian administrator No, scanned at user specified interval. Set to 0 to stop.
Set file specs and import interval from Historian Administrator. (Timestamps for data or messages may be at intervals less than the import interval.) Yes
Python Expression Tags No
Create Historian Tags Yes.
Note: The File Collector can be used to create Python Expression Tags for those collectors that support them. See the Python Expression Tags book for a list of collectors that support Python Expression Tags.
File Encoding ANSI