Configuration tab for File Collectors

Important: You do not have the latest version of Historian! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Historian product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GE Digital Sales Support. For the most up-to-date documentation, go here.

To display the Configuration tab for a File Collector, select a File Collector from the list on the left and click the Configuration Tab. The screen shown in the following figure appears.



Collector-Specific Configuration (File)

The Configuration tab displays the following information.

ThisField... Indicates...
Scan Interval The rate at which the input directory, Historian\ImportFiles, is scanned for any new files. To change it, enter a new value. The scan interval cannot exceed 65 seconds.
Note: Changes to the Scan Interval do not take effect until the File Collector is restarted
CSV File Specifications The file extension for the CSV file being imported. You can specify more than one extension type, such as: csv, txt, dat.
XML File Specification The file extension for the XML file being imported.
Purge Processed Files (days) The number of days a file can reside in the Processed Files directory before being deleted automatically.
Purge Error Files (days) The number of days an error file is retained before being deleted automatically. The default is 10.
String Data Yes