Use Parameterized Queries
Procedure
Use the following example code to use parameterized queries:
Private Sub SampleParameterizedQuery()
Dim ihConnectString As String
Dim ihRecordSet As ADODB.Recordset
Dim ihConnection As ADODB.Connection
Dim ihParameter As ADODB.Parameter
Dim ihCommand As ADODB.Command
'Set Up the Historian Connect String...
Set ihConnectString = "Provider=ihOLEDB.iHistorian.1;User Id=;Password="
'Create Our Other Objects...
Set ihConnection = CreateObject("ADODB.Connection")
Set ihRecordSet = CreateObject("ADODB.Recordset")
Set ihCommand = CreateObject("ADODB.Command")
'Open the Connection to the Historian Archiver...
ihConnection.ConnectionString = ihConnectString
ihConnection.Open
'Set up the Command Object
With ihCommand
'Set the Active Connection to the Historian Connection Opened Above..
.ActiveConnection = ihConnection
'Set the Command Text to a Parameterized Sql Statement....
.CommandText = "select * from ihTags where datatype = ?"
'Set the Type of the Command...
.CommandType = adCmdText
'Refresh Our Parameter List...
.Parameters.Refresh
End With
'Create a Single Parameter Object...
Set ihParameter = ihCommand.CreateParameter("Temp", adChar, adParamInput, 100)
'Set the Parameters Value...
ihParameter.Value = "SingleFloat"
'Add the Parameter to the Command Object...
ihCommand.Parameters.Append ihParameter
'Run the Command!
Set ihRecordSet = ihCommand.Execute
End Sub
For more information, refer to Parameterized SQL Queries.