Import Messages

About this task

You can import all the messages from an Excel worksheet into a Historian server. You can, however, only add messages to Historian; you cannot modify or remove them.

Procedure

  1. Open an Excel worksheet.
  2. Select Historian > Administration > Import Messages.
    A message appears, asking you to confirm that you want to import messages.
  3. Select Yes to execute the import. A window appears when the operation is complete. Select OK to close the window.
    A message appears, stating that the import is successful. If, however, an error occurs in any line of the import, the whole import is aborted.