Rename Enumerated Set

You can rename an enumerated set if needed.

Procedure

  1. Access Configuration Hub.
  2. In the NAVIGATION section, under the Configuration Hub plugin for Historian, select Tags.
  3. Select , and then select Manage Enumerated Sets.
    The Manage Enumerated Sets: <system name> window appears.
  4. Select the enumerated set that you want to rename.
    Details corresponding to the selected data set are displayed.
  5. In SET NAME, rename the name of the set.
  6. Select Save Set.
    The set name is renamed.
  7. Click Done.
    The changes are saved.