Configure FTP
Before you begin
About this task
Procedure
- Access the FTPFileTransfer file located in the <Installation folder of Historian ETL>/Historian ETL Transform folder.The FTP File Transfer Tool window appears.
- If the FTP configuration details are saved in a file, select , and then select the configuration file that contains the details. Otherwise, skip to the next step.
- Provide values as specified in the following table.Tip: You can select to create a new instance of the settings.
Field Description Default Value FTP Server Address Enter the address of the FTP server. ftp://127.0.0.1/ftpserver FTP UserID Enter the user ID to log in to the FTP server. Blank FTP Password Enter the password to log in to the FTP server. Blank Directory to Monitor Provide the folder from which files must be transferred. C:\ File Mask Enter the file mask for the FTP server. *.zip - Optional: Select Test Connection to test the FTP server connection.
- Select to save the configuration details, which you can reuse.
- Select if you want a detailed logging, which will help you in troubleshooting.