ihRawData Table
The ihRawData table contains any collected data for each tag contained in the Historian server. It contains not just raw data, but also calculated data and interpolated data. This table is the one typically used for reporting.
There is one row in the ihRawData table for each combination of tagname and timestamp. For instance, you can have two rows for the same tag, each with different timestamps. You can retrieve data for more than one tag name in a simple query.
The following table describes the columns of the ihRawData table.
Column Name | Data Type | Description |
---|---|---|
Tagname | VT_BSTR | Tagname property of the tag. Note: There is no length limit for Historian tag names in the Data Archiver. However, different client applications may have their own limits. |
TimeStamp | VT_DBTimeStamp | The date and time for the data sample. |
TimeStampSeconds | VT_DBTimeStamp | The date and time for the data sample. |
Microseconds | VT_DBTimeStamp | The microsecond interval for the data sample. |
Value | VT_VARIANT | The value of the data. |
Quality | VT_VARIANT | For non-raw sampled data, this column displays the percentage of good quality samples in the interval. For instance, a value of 100 means all samples in the interval are good.For raw sampled data, data values are:
|
OPCQualityValid | VT_BSTR | Indicates whether the OPCQuality column contains valid real OPC quality. A value of 0 indicates that you should ignore the OPCQuality field, and a value of 1 indicates that the OPCQuality column contains valid real OPC quality. |
OPCQuality | VT_I4 | Indicates the OPC quality as delivered by the OPC server to the Historian OPC collector. The exact meaning of the bits depends on the OPC specification and the OPC server documentation. Typically, a value of 0 represents bad quality, and a value of 192 represents good quality. |
SamplingMode | VT_BSTR | The mode used to sample data from the archive:
|
Direction | VT_BSTR | The direction (forward or backward from the start time) of data sampling from the archive. |
NumberOfSamples | VT_I4 | Number of samples from the archive to retrieve. Samples will be evenly spaced within the time range defined by the start and end times for most sampling modes. For the Note: The NumberofSamples and IntervalMilliseconds columns are mutually exclusive. If NumberofSamples is used, IntervalMilliseconds is not used. |
IntervalMilliseconds | VT_I4 | For non-raw sampled data, this column represents a positive integer for the time interval (in milliseconds) between returned samples. Note: The NumberofSamples and IntervalMilliseconds columns are mutually exclusive. If NumberofSamples is used, IntervalMilliseconds is not used. |
CalculationMode | VT_BSTR |
This column applies only if the
|
FilterTag | VT_BSTR | Tagname used to define the filter, if specified. Only a single tag can be specified, and wildcards are not supported. |
FilterMode | VT_BSTR | The type of time filter:
This mode defines how time periods before and after transitions in the filter condition should be handled. For example,AfterTime indicates that the filter condition should be True starting at the timestamp of the archive value that triggered the True condition and leading up to the timestamp of the archive value that triggered the False condition. |
FilterComparisonMode | VT_BSTR | The type of comparison to be made on the filter comparison value:
FilterTag value should be compared to the FilterValue value to establish the state of the filter condition. If FilterTag and FilterComparisonValue values are specified, time periods are filtered from the results where the filter condition is False . |
FilterValue | VT_BSTR | The value with which to compare the FilterTag value to determine appropriate filter times. |
FilterExpression | VT_BSTR | An expression which includes one or more filter conditions. The type of conditions used are:
FilterExpression can be used instead of the FilterTag , FilterComparisonMode and FilterValue parameters. While using FilterExpression , the expression is passed within single quotes. For complex expressions, write the conditions within parentheses. There is no maximum length for the FilterExpression value, but if called using OLE DB or Excel, those tools may have their own limitations. |
TimeZone | VT_BSTR | The type of time zone used:
|
DaylightSavingTime | VT_BOOL | Indicates whether Daylight Saving Time logic should be applied to timestamps. |
RowCount | VT_I4 | Indicates the maximum number of rows that can be returned. A value of 0 indicates that there is no limit to the number of rows returned. |
The ihRawData
table can generate a large number of rows if not used with caution. You can easily generate queries which take a very long time to complete and put stress on the archiver and generate network traffic.
ihRawData Examples
Tasks that you might want to perform on the ihRawData
table are outlined in the following examples.
Example 1: Retrieve All Samples With a Value Outside the Query Supplied Values
SELECT * FROM ihRawData WHERE value<140000 OR value>150000
Example 2: Retrieve All Bad Samples (Raw Data)
SELECT * FROM ihRawData WHERE quality NOT LIKE good*
AND samplingmode=RawbyTime
Example 3: Count Bad Samples (Raw Data)
SELECT COUNT(*) FROM ihRawData WHERE quality NOT LIKE good*
AND samplingmode=RawbyTime
Example 4: Retrieve All Bad Samples Over the Last Day (Interpolated Data)
SELECT timestamp, tagname, value, quality FROM ihRawData
WHERE samplingmode=rawbytime
AND Quality NOT LIKE good*
AND timestamp>=Now-24H
Example 5: Use an Explicit Time Zone
SELECT * FROM ihRawData WHERE timezone=300
Example 6: Perform a Simple Sequence of Events
SELECT timestamp, tagname, value, quality FROM ihrawdata
WHERE samplingmode=rawbytime ORDER BY timestamp
Example 7: Report the Busiest Tags
SELECT tagname, value FROM ihRawData
WHERE samplingmode=calculated
AND calculationmode=count
AND numberofsamples=1
AND timestamp>='07/30/2002 10:00:00'
AND timestamp<='07/30/2002 11:00:00' order by value descending
Example 8: Retrieve All Bad Samples Over the Last Day
SELECT timestamp, tagname, value, quality FROM ihRawData
WHERE samplingmode=rawbytime
AND Quality NOT LIKE good*
AND timestamp>=Now-24H
Example 9: Retrieve All Bad Samples, Ignore End of Collection Markers
SELECT timestamp, tagname, value, quality FROM ihRawData
WHERE samplingmode=rawbytime
AND Quality NOT LIKE good*
AND quality NOT LIKE 'bad offline' AND timestamp>=Now-24H
Example 10: Count Bad Samples, Ignore End of Collection Markers
SELECT COUNT(*) FROM ihRawData WHERE samplingmode=rawbytime
AND Quality NOT LIKE good* and Quality NOT LIKE 'bad offline'
AND timestamp>=Now-24H
Example 11: Obtain All Raw Samples With Comments From Yesterday
SELECT ihRawData.Tagname, ihRawData.TimeStamp, ihRawData.Value
FROM ihRawData
INNER JOIN ihComments ON ihComments.Tagname = ihRawData.Tagname
AND ihComments.Timestamp = ihRawData.Timestamp
AND ihComments.Comment = "The comment" WHERE samplingmode=rawbytime
AND ihComments.Timestamp > Yesterday
AND ihComments.Timestamp < Today
Example 12: Determine the Number of Milliseconds Per Interval With Good Data
SELECT timestamp, tagname, value as TimeGood, quality, intervalmilliseconds FROM ihRawData
WHERE tagname=Denali.Simulation00001
AND samplingmode=calculated
AND calculationmode=timegood
AND intervalmilliseconds=10s
AND timestamp>='1/20/2003 13:18:00'
AND timestamp<='1/20/2003 13:20:00'
Example 13: Retrieve Raw Minimum and Maximum Values Per Interval
In this example, you use the data retrieved from the query (with the Trend
sampling mode) to plot points.
SELECT timestamp, tagname, value, quality
FROM ihRawData
WHERE tagname=dFloatTag5
AND samplingmode=trend
AND intervalmilliseconds=24h
AND timestamp>='1/01/2003 07:00:00'
AND timestamp<='1/10/2003 12:00:00'
Example 14: Retrieve Data with Native Values and Tags Associated With Enumerated Sets
If the enumnativevalue
query modifier is not set, the data is
retrieved with string values by default. If it is set, the raw values are retrieved.
These values are then retrieved by default for the current session and will only
change when you open a new session.
SELECT * from ihrawdata
WHERE samplingmode='rawbytime' and tagname=mytag AND criteriastring='#enumnativevalue'
SELECT timestamp,value,quality from ihrawdata WHERE tagname = MyTag AND samplingmode=Interpolated and numberofsamples=6 and criteriastring='#enumnativevalue'
SET criteriastring='#enumnativevalue'
SELECT * from ihrawdata
WHERE samplingmode='rawbytime' and tagname=mytag
Example 15: Retrieve Average Values for Enumerated Sets
SET criteriastring='#enumnativevalue'
SELECT * from ihrawdata
WHERE tagname LIKE Call AND samplingmode=calculated AND calculationmode=average
Example 16: Retrieve RawAverage with an example of Good\Bad(positive\negative values)\End of Collection marker entry
In this example, we are using the #FilterIncludeBad#IncludeBad
modifier to include the Bad (positive) value. However, note that the
FILTERINCLUDEBAD
modifier considers bad quality data but
excludes Historian-injected end-of-collection markers, calculation errors, and
timeouts. This query will return all raw samples of all qualities with a timestamp
greater than the start time and less than or equal to the end time. It will not
return a raw sample with the same timestamp as the start time; therefore, provide a
timestamp just before the exact start timestamp. Additionally, include
>0 in the FilterExpression
to exclude
entries with a 0 bad value or a 0 bad end-of-collection marker.
SELECT value AS Val
FROM ihRawData
WHERE
ihRawData.TimeStamp >= '2024-10-30 17:08:35'
AND
ihRawData.TimeStamp <= '2024-10-30 17:09:12'
AND
ihRawData.Tagname = 'SIBAHISTWS2019_Simulation.Simulation00001'
AND
SamplingMode = 'calculated'
AND
CalculationMode = 'RawAverage'
AND
FilterExpression ='SIBAHISTWS2019_Simulation.Simulation00001>0'
AND
NumberofSamples = 1
AND
CriteriaString='#FilterIncludeBad#IncludeBad'
The following query serves as an example to determine the count or number of samples.
This query will return all raw samples of all qualities with a timestamp greater
than the start time and less than or equal to the end time. It will not include a
raw sample with a timestamp as the start time; therefore, provide a timestamp
slightly before the exact start timestamp. Additionally, include >0 in the
FilterExpression
to exclude entries with a bad value of 0 or a
0 indicating the end-of-collection marker.
SELECT value AS Val
FROM ihRawData
WHERE
ihRawData.TimeStamp >= '2024-10-30 17:08:35'
AND
ihRawData.TimeStamp <= '2024-10-30 17:09:12'
AND
ihRawData.Tagname = 'SIBAHISTWS2019_Simulation.Simulation00001'
AND
SamplingMode = 'calculated'
AND
CalculationMode = 'Count'
AND
FilterExpression ='SIBAHISTWS2019_Simulation.Simulation00001>0'
AND
NumberofSamples = 1
AND
CriteriaString='#FilterIncludeBad#IncludeBad'
In the following example, the query retrieves a count of 10 samples. However, for the average calculation, only 6 samples is considered. This is due to the exclusion of one end-of-collection marker, one bad value (0), and two negative values.