Examples: Using the Built-in Functions
Retrieving the Current value
You can use the current value function to retrieve the current value of an existing
Historian tag.
Result=Historian.CurrentValue('Tag1’)
Get the
current value of two tags and return the greater value of the two value:Return the Greater Value of Two Tags
x=Historian.CurrentValue('Tag1')
y=Historian.CurrentValue('Tag2')
if x > y:
Result= x
else:
Result= y
Add the Values of Two Tags
Result=Historian.CurrentValue(‘Tag1')+Historian.CurrentValue('Tag2')