0 |
ihSTATUS_OK |
The values have been successfully written to the tags. |
-1 |
ihSTATUS_FAILED |
The operation has failed. |
-2 |
ihSTATUS_API_ TIMEOUT |
The operation has timed out while connecting to Historian. |
-3 |
ihSTATUS_NOT_ CONNECTED |
The Calculation collector cannot connect to Historian. |
-4 |
ihSTATUS_INTERFACE_ NOT_FOUND |
You cannot connect to the Calculation collector. |
-5 |
ihSTATUS_NOT_ SUPPORTED |
The write operation is not supported. |
-6 |
ihSTATUS_DUPLICATE_ DATA |
The write operation has created duplicate data in the
archive. |
-7 |
ihSTATUS_NOT_VALID_ USER |
The username used to connect to the Historian archive is not valid. |
-8 |
ihSTATUS_ACCESS_ DENIED |
The username used to connect to Historian does not have write access to the archive. |
-9 |
ihSTATUS_WRITE_IN_ FUTURE |
The timestamp that you have entered is set to a time in
future. |
-10 |
ihSTATUS_WRITE_ ARCH_OFFLINE |
The archive is currently offline. |
-11 |
ihSTATUS_ARCH_ READONLY |
The archive is set to read-only. |
-12 |
ihSTATUS_WRITE_ OUTSIDE_ACTIVE |
An attempt has been made to write data to a time before the
archive has been created. |
-13 |
ihSTATUS_WRITE_NO_ ARCH_AVAIL |
No archive is available for writing. |
-14 |
ihSTATUS_INVALID_ TAGNAME |
The tag names that you have entered do not exist in the
archive. |
-15 |
ihSTATUS_LIC_TOO_MANY_TAGS |
You have attempted to add more tags than the current license
allows. |
-16 |
ihSTATUS_LIC_TOO_ MANY_USERS |
There are currently too many users connected to the
archive. |
-17 |
ihSTATUS_LIC_ INVALID_LIC_DLL |
The Historian license is expired or invalid. |
-18 |
ihSTATUS_NO_VALUE |
You have not entered a tag value. |
-19 |
ihSTATUS_DUPLICATE_ INTERFACE |
Two collectors with the same name exist. |
-20 |
ihSTATUS_NOT_ LICENSED |
The Historian license is not activated. |
-21 |
ihSTATUS_CALC_CIRC_ REFERENCE |
A circular reference has been entered in the calculation
formula. |
-22 |
ihSTATUS_BACKUP_ EXCEEDED_SPACE |
The archive has reached the Minimum Hard Drive Space setting, and
no new archives are being created. |
-23 |
ihSTATUS_INVALID_ SERVER_VERSION |
The archive is not compatible with the Calculation collector. |
-24 |
ihSTATUS_DATA_ RETRIEVAL_COUNT_ EXCEEDED |
There are too many data points to retrieve. |