Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / OnCollectorControlResponse Method
Indication of how the request was processed.



In This Topic
    OnCollectorControlResponse Method
    In This Topic
    Invoked by the remote server to transmit the result of a control request.
    Syntax
    'Declaration
     
    Public Sub OnCollectorControlResponse( _
       ByVal status As Status _
    ) 
    'Usage
     
    Dim instance As ServerConnection
    Dim status As Status
     
    instance.OnCollectorControlResponse(status)
    public void OnCollectorControlResponse( 
       Status status
    )
    public:
    void OnCollectorControlResponse( 
       Status status
    ) 

    Parameters

    status
    Indication of how the request was processed.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also