Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IEnumeratedSets Interface / Set Method
EnumeratedSet to update.



In This Topic
    Set Method (IEnumeratedSets)
    In This Topic
    Apply properties from the given set to a Historian server.
    Syntax
    'Declaration
     
    Sub Set( _
       ByVal enumeratedSet As EnumeratedSet _
    ) 
    'Usage
     
    Dim instance As IEnumeratedSets
    Dim enumeratedSet As EnumeratedSet
     
    instance.Set(enumeratedSet)
    void Set( 
       EnumeratedSet enumeratedSet
    )
    void Set( 
       EnumeratedSet^ enumeratedSet
    ) 

    Parameters

    enumeratedSet
    EnumeratedSet to update.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also