Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IEnumeratedSets Interface / Add Method
Contains a unique enumerated set name, and other properties.



In This Topic
    Add Method (IEnumeratedSets)
    In This Topic
    Add an enumerated set to a Historian server.
    Syntax
    'Declaration
     
    Sub Add( _
       ByVal enumeratedSet As EnumeratedSet _
    ) 
    'Usage
     
    Dim instance As IEnumeratedSets
    Dim enumeratedSet As EnumeratedSet
     
    instance.Add(enumeratedSet)
    void Add( 
       EnumeratedSet enumeratedSet
    )
    void Add( 
       EnumeratedSet^ enumeratedSet
    ) 

    Parameters

    enumeratedSet
    Contains a unique enumerated set name, and other properties.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also