Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / IArchives Interface / Set Method
Archive properties to apply.



In This Topic
    Set Method (IArchives)
    In This Topic
    Set the properties of an archive in a Historian server. Archives are uniquely identifed by name.
    Syntax
    'Declaration
     
    Sub Set( _
       ByVal archive As Archive _
    ) 
    'Usage
     
    Dim instance As IArchives
    Dim archive As Archive
     
    instance.Set(archive)
    void Set( 
       Archive archive
    )
    void Set( 
       Archive^ archive
    ) 

    Parameters

    archive
    Archive properties to apply.
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also