Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / EnumeratedSet Class / NumberOfStates Property



In This Topic
    NumberOfStates Property
    In This Topic
    Number of states in the set
    Syntax
    'Declaration
     
    <DataMemberAttribute("NumberOfStates")>
    Public Property NumberOfStates As Integer
    'Usage
     
    Dim instance As EnumeratedSet
    Dim value As Integer
     
    instance.NumberOfStates = value
     
    value = instance.NumberOfStates
    [DataMember("NumberOfStates")]
    public int NumberOfStates {get; set;}
    [DataMember("NumberOfStates")]
    public:
    property int NumberOfStates {
       int get();
       void set (    int value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also