Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / EnumeratedSet Class / Description Property



In This Topic
    Description Property (EnumeratedSet)
    In This Topic
    Set Description
    Syntax
    'Declaration
     
    <DataMemberAttribute("Description")>
    Public Property Description As String
    'Usage
     
    Dim instance As EnumeratedSet
    Dim value As String
     
    instance.Description = value
     
    value = instance.Description
    [DataMember("Description")]
    public string Description {get; set;}
    [DataMember("Description")]
    public:
    property String^ Description {
       String^ get();
       void set (    String^ value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also