Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / CalculatedQuality Class / BadPercent Field



In This Topic
    BadPercent Field
    In This Topic
    Percent value representing bad quality.
    Syntax
    'Declaration
     
    Public Const BadPercent As Single
    'Usage
     
    Dim value As Single
     
    value = CalculatedQuality.BadPercent
    public const float BadPercent
    public:
    const float BadPercent
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also