Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmFields Class / AlarmId Property



In This Topic
    AlarmId Property (AlarmFields)
    In This Topic
    Syntax
    'Declaration
     
    <DataMemberAttribute("AlarmId")>
    Public Property AlarmId As AlarmField
    'Usage
     
    Dim instance As AlarmFields
    Dim value As AlarmField
     
    instance.AlarmId = value
     
    value = instance.AlarmId
    [DataMember("AlarmId")]
    public AlarmField AlarmId {get; set;}
    [DataMember("AlarmId")]
    public:
    property AlarmField^ AlarmId {
       AlarmField^ get();
       void set (    AlarmField^ value);
    }
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also