Windows Performance Collector Feature Summary
The following table outlines the features of the Windows Performance Collector.
Feature | Capability |
---|---|
Minimum Poll Interval | Yes- 1 second |
Unsolicited Collection | No |
Timestamp Resolution | Yes- 1 millisecond |
Accept Device Timestamps | No |
Floating Point Data | Yes |
Integer Data | Yes |
String Data | Yes |
Binary Data | No |
Collector Compression | Yes |
Reads data, tags | Yes |
Start/stop collection from the system | Yes |
Condition based Collection Support | No |
Python Expression Tags | Yes |
Note: Though the Minimum Poll Interval supported by the Windows Performance Collector is 1 second, it is recommended to set the interval to 5 seconds when adding large number of tags for proper collection of data.