Modify a Query

About this task

You can change query parameters such as tag name, start time, end time, and so on. You cannot, however, narrow down the output range. For example, you cannot reduce the number in the NumberOfSamples field, or you cannot change the Output Orientation to values that result in fewer rows or columns.

Procedure

  1. Open an Excel worksheet.
  2. Access the query that you want to modify.
  3. In the Add-In drop-down list box, select Edit Query or icon. Or you can double-click any cell that has the query formula.
    The Edit Query window appears.
  4. Modify the query, and then select OK.