Managing Enumerated Sets
Before You Begin
Export the enumerated sets into an Excel worksheet.To add sets:
- Enter details in the following columns in the Excel worksheet.
- SetName
- SetDescription
- StateName
- StateDescription
- StateLowValue
- StateHighValue
- StateRawValueDataType
- NumberOfStatesInThisSet
- Select Import Enumerated Sets.
To delete sets:
- Select the row that contains the state you want to delete.
- Right-click the row, and then select Delete.
To modify the description of a set:
Place the cursor in the StateDescription cell and modify the description.
You cannot modify the name of the set. If you change the name of the set, it is considered a new set.
To add states:
- Select the set to which you want to add a set.
- Add the name of the set in the SetName column.
The name match the set you selected.
- Enter the details in the SetDescription, StateName, StateDescription, StateLowValue, StateHighValue, and StateRawValueDataType columns.
- Enter the total number of states in the NumberOfStatesInThisSet column.
Ensure that this value is the same for the current state and existing states in the set. For example, if a state has two states already and you are adding a third state, the number of states for all the three states must be changed to three.
A new state is added to the set.
To modify states:
- Modify the values of each state.
The states are modified.
To delete states:
- Select the row that contains the state you want to delete.
- Right-click the row, and then select Delete.
The state is deleted.