Create a Sample JSON File
About this task
Procedure
-
Run the RemoteCollectorConfigurator.exe file. By default,
it is located in the following folder: C:\Program Files\GE
Digital\NonWebCollectorInstantiationTool\RemoteCollectorConfigurator.exe.
A list of options to manage collector instances appears.
-
Enter 7.
A list of collector types appears, along with a number assigned to each of them. You are prompted to enter the collector type.
-
Specify the collector type by entering the corresponding number. For
example, if you want to add an instance of the Calculation collector, enter 1.
A list of destinations appears, along with a number assigned to each of them.
- Specify the destination by entering the corresponding number. For example, if the destination is a Historian server, enter 1.
-
If needed, enter the folder path where you want the sample JSON file to be
created. By default, the file will be created in the same folder in which the
RemoteCollectorConfigurator utility is located.
A sample JSON file is created.
- As needed, update the sample JSON file with the required collector instance parameters. You can also specify values for the general parameters.