Delete an Offline Collector Instance

About this task

This topic describes how to delete an offline collector instance using the RemoteCollectorConfigurator utility.
Note: When you delete an offline collector instance, the corresponding configuration file is not deleted. However, if another collector instance of the same interface name is created, the existing configuration file is replaced by a template configuration file.

Procedure

  1. Access the installation folder of the RemoteCollectorConfigurator utility. By default, it is C:\Program Files\GE Digital\NonWebCollectorInstantiationTool.
  2. Run the RemoteCollectorConfigurator.exe file. By default, it is located in the following folder: .
  3. Run the following command:
    ihCollectorManager_x64.exe InterfaceDelete <interface name>