Set a Default Data Store

About this task

A default data store is the one that is considered if you do not specify a data store while adding a tag.

Procedure

  1. Access Configuration Hub.
  2. In the NAVIGATION section, select Systems.
  3. Select the system whose default data store you want to change.
    The details of the system appear in the DETAILS section.
  4. Under System Defaults, next to Default Data Store, select .
    The Default Data Store: <system name> window appears.
  5. Select the data store that you want to set as default, and then select Set as Default.
    The default data store of the system is changed.