Have You Seen Historian Lately?Click here to check out all the new features in the latest version.
Supercharge your GE solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Learn more about the Proficy 2022 releases, by signing up for one of our upcoming events.
Connect to the OLE DB provider, and add the Historian database tables.
About this task
To format decimal point precision in your reports, you
must convert Variant data types to Float data types in Crystal Reports. For instance, if
retrieving the Value column from the ihRawData table, you must convert the values to
Float. You need not perform these steps if you are working with strings.
Procedure
Access Standard Report Expert, and then select
Fields.
The Fields section appears.
Select Formula.
The Formula Name window appears.
Enter a name for the formula.
The Formula Editor section appears.
Tip: You can also access the Formula Editor section by
selecting Insert > Field Object. Right-click the formula fields, and then select
New.
In the Formula field, enter the following text :
if numerictext({ihRawData.Value}) then cdbl({ihRawData.Value}) else
0
Select Save.
You can now use the formula as a normal numeric column instead of the
Value column in the report.