Have You Seen Historian Lately?Click here to check out all the new features in the latest version.
Supercharge your GE solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Learn more about the Proficy 2022 releases, by signing up for one of our upcoming events.
To generate reports in Crystal Reports, you must ensure that the Historian Server name is
correct. By default, this server name is
T20.
Procedure
Open the report file in Crystal Reports.
Select the Database menu.
If the Database menu
does not appear automatically:
Wait for approximately 90 seconds for the
connection timeout to occur.
After the 90-second timeout, the
Data Link Properties window
appears. Although it may appear as if Crystal
Reports has stopped working or is frozen before
the timeout occurs, this functionality is as
expected.
Change the Data Source
field.
You can leave this field empty to use the
default Historian server or enter a specific
Historian server name.
Select OK.
Skip the next step.
If the Database menu
appears automatically:
Select Database > Set Location.
The Set Location
window appears.
Select Set
Location.
The Data Explorer
window appears.
Select a source, and then select
Set.
Select Done.
Results
The Historian server is connected with
Crystal Reports.