Configure the Simulation Collector Using Historian Administrator

Before you begin

Install collectors, and create an instance of the collector.

Procedure

  1. Access Configuration Hub.
  2. Select Collectors, and then select the Simulation collector instance that you want to configure.
    The fields specific to the collector instance appear.

  3. Enter values as specified in the following table.
    Field Description
    Number of Tags The number of Historian tags that you want the create for the collector.
    Function Period (seconds) The period, in seconds, of the SIN,STEP, and RAMP functions implemented in the collector.
  4. As needed, enter values in the other sections.
  5. Restart the collector.
    The collector instance is configured.