Have You Seen Historian Lately?Click here to check out all the new features in the latest version.
Supercharge your GE solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Learn more about the Proficy 2022 releases, by signing up for one of our upcoming events.
You can reconnect to the ODBC server automatically as soon as the server is up and running.
By default, the collector polls for the server connection every 5
seconds. You can change this interval as well. The collector is
stopped until reconnected to the server.
Procedure
Access the following registry key:
HKEY_LOCAL_MACHINE\SOFTWARE\GE
Digital\iHistorian\Services\ODBCCollector.
Create a DWORD named
EnableReconnect.
Enter the decimal value 1.
If you want to change the reconnection interval (from
the default value of 5 seconds):
Create a DWORD named
ReconnectInterval.
Enter a decimal value between 5 and 60. This
value represents the number of seconds for the
collector to wait before trying to reconnect to
the ODBC server.