Troubleshooting ETL Issues
Unable to Start the ETL Tools
Issue: When you try to start the Historian ETL Extract, Historian ETL PI Extract, or the Historian ETL Load service, an error occurs.
- Access the configuration file for the service that you want to start. For example, for the Historian ETL Extract service, access the HistorianETLExtract.exe.config file.
- Set the element generatePublisherEvidence to disabled.
An Error Occurs When Importing Tag Data into an Excel Spreadsheet
Issue: To specify tags using a template spreadsheet, when you import the tags stored in an .xml file, an error occurs, stating that the data is not valid according to the schema.
- You have provided values in all the red-colored columns.
- Values in the Name column are unique.
- There are no blank rows.
- The values that you have entered are valid and of the same data type as defined for each property.
Issue: When you attempt to import tag data to an Excel spreadsheet from an .xml file, an error occurs, stating that the .xml file is not linked to schema.
Workaround: Ignore the message.