Example of a Regeneration File
The following lines of code represent the content of a regeneration file, which provides the start time, end time, and interval to export data. After all the requests are processed, the regeneration file is deleted.
Note: The regeneration file has three sections for setting the start time, end time, and interval. These multiple sections act as a backup. That is, if the values provided in the first section are not valid (for example, the start time is later than the end time, interval has a negative value), the values from the next section are considered.
<?xml version="1.0"?>
<SOAP-ENV:Envelope xmlns:xsi="http://www.w3.org/2001/XMLSchema-instance" xmlns:xsd="http://www.w3.org/2001/XMLSchema" xmlns:SOAP-ENC="http://schemas.xmlsoap.org/soap/encoding/" xmlns:SOAP-ENV="http://schemas.xmlsoap.org/soap/envelope/" xmlns:clr="http://schemas.microsoft.com/soap/encoding/clr/1.0" SOAP-ENV:encodingStyle="http://schemas.xmlsoap.org/soap/encoding/">
<SOAP-ENV:Body>
<a1:ArrayList id="ref-1" xmlns:a1="http://schemas.microsoft.com/clr/ns/System.Collections">
<_items href="#ref-2"/>
<_size>3</_size>
<_version>3</_version>
</a1:ArrayList>
<SOAP-ENC:Array id="ref-2" SOAP-ENC:arrayType="xsd:anyType[4]">
<item href="#ref-3"/>
<item href="#ref-4"/>
<item href="#ref-5"/>
</SOAP-ENC:Array>
<a3:RegenRequest id="ref-3" xmlns:a3="http://schemas.microsoft.com/clr/nsassem/ETLExtract/HistorianETLExtract%2C%20Version%3D1.9.0.0%2C%20Culture%3Dneutral%2C%20PublicKeyToken%3Dnull">
<startTime>2020-07-02T09:39:37.3384336+05:30</startTime>
<endTime>2020-07-02T10:39:37.3384336+05:30</endTime>
<interval>3</interval>
</a3:RegenRequest>
<a3:RegenRequest id="ref-4" xmlns:a3="http://schemas.microsoft.com/clr/nsassem/ETLExtract/HistorianETLExtract%2C%20Version%3D1.9.0.0%2C%20Culture%3Dneutral%2C%20PublicKeyToken%3Dnull">
<startTime>2020-07-02T09:39:37.3384336+05:30</startTime>
<endTime>2020-07-02T10:39:37.3384336+05:30</endTime>
<interval>4.5</interval>
</a3:RegenRequest>
<a3:RegenRequest id="ref-5" xmlns:a3="http://schemas.microsoft.com/clr/nsassem/ETLExtract/HistorianETLExtract%2C%20Version%3D1.9.0.0%2C%20Culture%3Dneutral%2C%20PublicKeyToken%3Dnull">
<startTime>2020-07-02T09:39:37.3384336+05:30</startTime>
<endTime>2020-07-02T10:39:37.3384336+05:30</endTime>
<interval>14.5</interval>
</a3:RegenRequest>
</SOAP-ENV:Body>
</SOAP-ENV:Envelope>