Configuring Custom Blocks
- block-name.gov
- block-name_details.json
In the above examples, block-name is the name of the custom block (e.g., for the D16 block, the files would be named D16.gov and D16_details.json).
When using the block tool kit to create custom blocks, the utility creates the .gov file; it is up to the user to create the .json file and save it in the C:\Program Files (x86)\GE\iFIX\PDB\ folder.
type_name
: the name of the custom block (e.g.,"type_name": "D16"
)- Category elements outline the logical groupings of items in the details
display. Using the D16 block as an example, its categories are
General
,IO_Addressing
,Device_States
,Alarms_Options
,E-Signature
, andAdvanced_Options
. Within each of these elements, there is a Rank entry that specifies the display order. For example:“rank”: 1
will display at the top of the details pane"rank": 2
will display next, etc.
General
heading of the D16 block
are:"General": [
{
"A_TAG": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.tagName"
]
}
},
{
"A_DESC": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"rank": 2
}
The behavior of display and input is controlled by these entries. In this example, the
tag name (“A_TAG”
) and description (“A_DESC”
) are
listed in the General
category. These must correspond to actual field
names available in the block. A complete list of field names and their descriptions can
be obtained by creating the custom blocks in the iFIX Databasemanager and exporting the
resulting PDB file to a CSV file, which can be opened (e.g., using Excel) to list the
field names and their corresponding descriptions.
“datatype”
, such as “string”
or
“number”
, and can be given an enumeration set to limit the values
entered to those defined in the enumeration set. The possible values will display as a
drop-down list for the field. A sample of this is demonstrated in the E-Signature
section of the D16_details.json file (at the bottom of this
page)."enum": [
"YES",
"NO"
]
- Additionally, validation criteria can be provided to stipulate allowable entries
for each field. This behavior is controlled by the “validators” section for the
tag field. Some commonly used validators are:
TagCommonValidators.maxLength
: Verifies that the value does not exceed the field’s maximum length, which is obtained from the .gov file. For example,field_length
is used to determine the length (fortagname
it will be 256).TagCommonValidators.tagName
: Checks for the tag name characters and matches the validation to that in the iFIX Databasemanager. It also checks for duplicates in the current database. For example, the following special characters cannot be in the iFIX tag name - ~ ` + ^ : ? " * = { } . , ; ? @TagCommonValidators.ioAddress
: This validator applies only to the SIM driver. The value cannot be more than 2000; if a bit value is used, it cannot be more than 15.TagCommonValidators.isIntegerValidation
: Checks if it is a numeric value, otherwise the input is rejected.TagCommonValidators.minValue
: Based on the value offield_min
in the .gov file.TagCommonValidators.maxValue
: Based on the value offield_max
in the .gov file.TagCommonValidators.isEmpty
: Checks if the value is empty.TagCommonValidators.scanTime
: Matches to the iFIX Databasemanager input for scan time.TagCommonValidators.blockName
: Similar totagName
, but does not check for a duplicate tag name in the database.TagCommonValidators.maxPrecision
: Based on the value offield_precision
in the .gov file.TagCommonValidators.eguValuesNotEqual
: This validator checks if the value is within EGU limits. If the value matches EGU limit values, it is rejected.TagCommonValidators.inValidNumericFormat
: Confirms that the number format matches the locale. Only default number formats for a given locale are supported.
TXT_details.json
{
"tag_type": [
{
"type_name": "TXT",
"category": {
"General": [
{
"A_TAG": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.tagName"
]
}
},
{
"A_DESC": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"rank": 1
}
],
"IO_Addressing": [
{
"A_IODV": {
"default": "SIM",
"enum": [
""
],
"datatype": "string"
}
},
{
"A_IOAD": {
"default": "0",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.ioAddress"
]
}
},
{
"A_IOSC": {
"default": "None",
"drivers": [],
"enum": [
""
],
"datatype": "string"
}
},
{
"A_IOHT": {
"default": "None",
"enum": [
"None"
],
"datatype": "string"
}
},
{
"rank": 2
}
],
"Limits_and_Scaling": [
{
"A_ELO": {
"default": "0.00",
"field_min": "-3.4E+38",
"field_max": "3.4E+38",
"field_precision": "16",
"enum": "",
"datatype": "number",
"validators": [
"TagCommonValidators.minValue",
"TagCommonValidators.maxValue",
"TagCommonValidators.maxPrecision",
"TagCommonValidators.isEmpty",
"TagCommonValidators.eguValuesNotEqual"
]
}
},
{
"A_EHI": {
"default": "100.00",
"field_min": "-3.4E+38",
"field_max": "3.4E+38",
"field_precision": "16",
"enum": "",
"datatype": "number",
"validators": [
"TagCommonValidators.minValue",
"TagCommonValidators.maxValue",
"TagCommonValidators.maxPrecision",
"TagCommonValidators.isEmpty",
"TagCommonValidators.eguValuesNotEqual"
]
}
},
{
"A_EGUDESC": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"rank": 3
}
],
"Text Strings": [
{
"TR0": {
"default": "1",
"field_min": "1",
"field_max": "65535",
"enum": "",
"datatype": "number",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.isIntegerValidation",
"TagCommonValidators.minValue",
"TagCommonValidators.maxValue"
]
}
},
{
"A_TS0": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"TR1": {
"default": "2",
"field_min": "1",
"field_max": "65535",
"enum": "",
"datatype": "number",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.isIntegerValidation",
"TagCommonValidators.minValue",
"TagCommonValidators.maxValue"
]
}
},
{
"A_TS1": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"TR2": {
"default": "4",
"field_min": "1",
"field_max": "65535",
"enum": "",
"datatype": "number",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.isIntegerValidation",
"TagCommonValidators.minValue",
"TagCommonValidators.maxValue"
]
}
},
{
"A_TS2": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"TR3": {
"default": "8",
"field_min": "1",
"field_max": "65535",
"enum": "",
"datatype": "number",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.isIntegerValidation",
"TagCommonValidators.minValue",
"TagCommonValidators.maxValue"
]
}
},
{
"A_TS3": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"TR4": {
"default": "16",
"field_min": "1",
"field_max": "65535",
"enum": "",
"datatype": "number",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.isIntegerValidation",
"TagCommonValidators.minValue",
"TagCommonValidators.maxValue"
]
}
},
{
"A_TS4": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"TR5": {
"default": "32",
"field_min": "1",
"field_max": "65535",
"enum": "",
"datatype": "number",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.isIntegerValidation",
"TagCommonValidators.minValue",
"TagCommonValidators.maxValue"
]
}
},
{
"A_TS5": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"TR6": {
"default": "64",
"field_min": "1",
"field_max": "65535",
"enum": "",
"datatype": "number",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.isIntegerValidation",
"TagCommonValidators.minValue",
"TagCommonValidators.maxValue"
]
}
},
{
"A_TS6": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"TR7": {
"default": "128",
"field_min": "1",
"field_max": "65535",
"enum": "",
"datatype": "number",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.isIntegerValidation",
"TagCommonValidators.minValue",
"TagCommonValidators.maxValue"
]
}
},
{
"A_TS7": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"TR8": {
"default": "256",
"field_min": "1",
"field_max": "65535",
"enum": "",
"datatype": "number",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.isIntegerValidation",
"TagCommonValidators.minValue",
"TagCommonValidators.maxValue"
]
}
},
{
"A_TS8": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"TR9": {
"default": "512",
"field_min": "1",
"field_max": "65535",
"enum": "",
"datatype": "number",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.isIntegerValidation",
"TagCommonValidators.minValue",
"TagCommonValidators.maxValue"
]
}
},
{
"A_TS9": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"TR10": {
"default": "1024",
"field_min": "1",
"field_max": "65535",
"enum": "",
"datatype": "number",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.isIntegerValidation",
"TagCommonValidators.minValue",
"TagCommonValidators.maxValue"
]
}
},
{
"A_TS10": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"TR11": {
"default": "2048",
"field_min": "1",
"field_max": "65535",
"enum": "",
"datatype": "number",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.isIntegerValidation",
"TagCommonValidators.minValue",
"TagCommonValidators.maxValue"
]
}
},
{
"A_TS11": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"TR12": {
"default": "4096",
"field_min": "1",
"field_max": "65535",
"enum": "",
"datatype": "number",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.isIntegerValidation",
"TagCommonValidators.minValue",
"TagCommonValidators.maxValue"
]
}
},
{
"A_TS12": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"TR13": {
"default": "8192",
"field_min": "1",
"field_max": "65535",
"enum": "",
"datatype": "number",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.isIntegerValidation",
"TagCommonValidators.minValue",
"TagCommonValidators.maxValue"
]
}
},
{
"A_TS13": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"TR14": {
"default": "16384",
"field_min": "1",
"field_max": "65535",
"enum": "",
"datatype": "number",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.isIntegerValidation",
"TagCommonValidators.minValue",
"TagCommonValidators.maxValue"
]
}
},
{
"A_TS14": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"TR15": {
"default": "32768",
"field_min": "1",
"field_max": "65535",
"enum": "",
"datatype": "number",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.isIntegerValidation",
"TagCommonValidators.minValue",
"TagCommonValidators.maxValue"
]
}
},
{
"A_TS15": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_TS16": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"rank": 4
}
],
"E-Signature": [
{
"A_ESIGTYPE": {
"default": "NONE",
"enum": [
"NONE",
"PERFONLY",
"PERFVERI"
],
"datatype": "string"
}
},
{
"A_ESIGCONT": {
"default": "YES",
"enum": [
"YES",
"NO"
],
"datatype": "string"
}
},
{
"A_ESIGACK": {
"default": "NO",
"enum": [
"YES",
"NO"
],
"datatype": "string"
}
},
{
"A_ESIGREQ_COMMENT": {
"default": "NO",
"enum": [
"YES",
"NO"
],
"datatype": "string"
}
},
{
"A_ESIGTRAP": {
"default": "REJECT",
"enum": [
"REJECT",
"ACCEPT",
"LOG"
],
"datatype": "string"
}
},
{
"rank": 5
}
],
"Advanced_Options": [
{
"A_OUT": {
"default": "NO",
"enum": [
"YES",
"NO"
],
"datatype": "string"
}
},
{
"A_CASE": {
"default": "NO",
"enum": [
"YES",
"NO"
],
"datatype": "string"
}
},
{
"Security_Areas": {
"default": "NONE",
"enum": [
""
],
"datatype": "string",
"applies_to": [
"A_SA1",
"A_SA2",
"A_SA3"
]
}
},
{
"A_SA1": {
"default": "NONE",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_SA2": {
"default": "NONE",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_SA3": {
"default": "NONE",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_ALMEXT1": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_ALMEXT2": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"rank": 6
}
]
}
}
]
}
D16_details.json
{
"tag_type": [
{
"type_name": "D16",
"category": {
"General": [
{
"A_TAG": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.tagName"
]
}
},
{
"A_DESC": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"rank": 1
}
],
"IO_Addressing": [
{
"A_MODE": {
"default": "A",
"enum": [
"A",
"D"
],
"datatype": "string"
}
},
{
"A_IODV": {
"default": "SIM",
"enum": [
""
],
"datatype": "string"
}
},
{
"A_IOAD": {
"default": "0",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.ioAddress"
]
}
},
{
"A_COUNT": {
"default": "16",
"enum": "",
"datatype": "string",
"field_min": "1",
"field_max": "16",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.isIntegerValidation",
"TagCommonValidators.minValue",
"TagCommonValidators.maxValue",
"TagCommonValidators.isEmpty"
]
}
},
{
"A_IOHT": {
"default": "None",
"enum": [
"None"
],
"datatype": "string"
}
},
{
"A_SCANT": {
"default": "1",
"enum": "",
"ProcessByException": "",
"PhaseAt": "",
"datatype": "number",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.scanTime"
]
}
},
{
"rank": 2
}
],
"Device_States": [
{
"A_LABEL[00]": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AE[00]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_INVERT[00]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_LABEL[01]": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AE[01]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_INVERT[01]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_LABEL[02]": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AE[02]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_INVERT[02]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_LABEL[03]": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AE[03]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_INVERT[03]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_LABEL[04]": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AE[04]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_INVERT[04]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_LABEL[05]": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AE[05]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_INVERT[05]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_LABEL[06]": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AE[06]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_INVERT[06]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_LABEL[07]": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AE[07]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_INVERT[07]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_LABEL[08]": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AE[08]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_INVERT[08]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_LABEL[09]": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AE[09]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_INVERT[09]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_LABEL[10]": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AE[10]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_INVERT[10]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_LABEL[11]": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AE[11]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_INVERT[11]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_LABEL[12]": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AE[12]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_INVERT[12]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_LABEL[13]": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AE[13]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_INVERT[13]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_LABEL[14]": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AE[14]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_INVERT[14]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_LABEL[15]": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AE[15]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"A_INVERT[15]": {
"default": "N",
"enum": [
"Y",
"N"
],
"datatype": "string"
}
},
{
"rank": 3
}
],
"Alarms_Options": [
{
"Alarm_Areas": {
"default": "ALL",
"enum": [
""
],
"datatype": "string",
"applies_to": [
"A_AREA1",
"A_AREA2",
"A_AREA3",
"A_AREA4",
"A_AREA5",
"A_AREA6",
"A_AREA7",
"A_AREA8",
"A_AREA9",
"A_AREA10",
"A_AREA11",
"A_AREA12",
"A_AREA13",
"A_AREA14",
"A_AREA15"
]
}
},
{
"A_IENAB": {
"default": "ENABLE",
"enum": [
"DISABLE",
"ENABLE"
],
"datatype": "string"
}
},
{
"A_PRI": {
"default": "LOW",
"enum": [
"INFO",
"LOW",
"LOLO",
"MEDIUM",
"HIGH",
"HIHI",
"CRITICAL"
],
"datatype": "string"
}
},
{
"A_AREA1": {
"default": "ALL",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AREA2": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AREA3": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AREA4": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AREA5": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AREA6": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AREA7": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AREA8": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AREA9": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AREA10": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AREA11": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AREA12": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AREA13": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AREA14": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_AREA15": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_IALMSHLVENAB": {
"default": "DISABLE",
"enum": [
"ENABLE",
"DISABLE"
],
"datatype": "string"
}
},
{
"A_ALMSHELVEPOLICY": {
"default": "",
"enum": [
""
],
"datatype": "string"
}
},
{
"rank": 4
}
],
"E-Signature": [
{
"A_ESIGTYPE": {
"default": "NONE",
"enum": [
"NONE",
"PERFONLY",
"PERFVERI"
],
"datatype": "string"
}
},
{
"A_ESIGCONT": {
"default": "YES",
"enum": [
"YES",
"NO"
],
"datatype": "string"
}
},
{
"A_ESIGACK": {
"default": "NO",
"enum": [
"YES",
"NO"
],
"datatype": "string"
}
},
{
"A_ESIGREQ_COMMENT": {
"default": "NO",
"enum": [
"YES",
"NO"
],
"datatype": "string"
}
},
{
"A_ESIGTRAP": {
"default": "REJECT",
"enum": [
"REJECT",
"ACCEPT",
"LOG"
],
"datatype": "string"
}
},
{
"rank": 5
}
],
"Advanced_Options": [
{
"A_ISCAN": {
"default": "ON",
"enum": [
"ON",
"OFF"
],
"datatype": "string"
}
},
{
"A_REALM": {
"default": "YES",
"enum": [
"YES",
"NO"
],
"datatype": "string"
}
},
{
"Security_Areas": {
"default": "NONE",
"enum": [
""
],
"datatype": "string",
"applies_to": [
"A_SA1",
"A_SA2",
"A_SA3"
]
}
},
{
"A_SA1": {
"default": "NONE",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_SA2": {
"default": "NONE",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_SA3": {
"default": "NONE",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_PREV": {
"default": "",
"enum": "",
"validators": []
}
},
{
"A_NEXT": {
"default": "",
"enum": "",
"validators": [
"TagCommonValidators.maxLength",
"TagCommonValidators.blockName"
]
}
},
{
"A_ALMEXT1": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"A_ALMEXT2": {
"default": "",
"enum": "",
"datatype": "string",
"validators": [
"TagCommonValidators.maxLength"
]
}
},
{
"rank": 6
}
]
}
}
]
}