Reconnecting to the Wonderware Server
About this task
To enable Auto-Reconnect to the Wonderware Server:
Procedure
- From the Start menu, select Run and type Regedit, then, select OK. The Registry Editor appears.
- Open the key folder: HKEY_LOCAL_MACHINE\SOFTWARE\GE Digital\iHistorian\Services\ WonderwareCollector.
- Create a new DWORD labelled, EnableReconnect.
- Enter the decimal value 1.
- Select OK, then close the Registry Editor.
- Restart the Historian Data Collector for Wonderware for the change to take effect.Important: If this registry is not created and set to a value of 1, then the auto-reconnect functionality will not be enabled.To configure the timer:
- From the Start menu, select Run and type Regedit. Then, select OK. The Registry Editor appears.
- Open the key folder: HKEY_LOCAL_MACHINE\SOFTWARE\GE Digital\iHistorian\Services\ WonderwareCollector.
- Create a new DWORD labelled, ReconnectInterval.
- Enter a decimal value greater than 5. This value represents the number of seconds for the collector to wait before trying to re-connect to the Wonderware Server.
- Select OK, and then edit the Registry Editor. Min Value = 5 seconds (default) Max Value = 60 seconds
- Select OK, and then edit the Registry Editor.
- Restart the Wonderware Collector for the change to take effect.