Configuring Wonderware Collector

Collector-Specific Configuration for the Wonderware Collector
Enter the value for the Wonderware Collector-specific field parameters:
Field | Description |
---|---|
Server Name |
Wonderware Server InSQL Database Server name. |
User Name |
Wonderware Server InSQL Database User name, for example, wwUser. |
Password |
Wonderware Server InSQL Database password, for example, XXXXXX. |
Recovery Time (hours) | Recovery logic is activated when the Wonderware Collector and Wonderware Historian
re-establish a connection after a connection loss, or when the
Wonderware Collector is started. The Wonderware Collector attempts to recover all data samples between the current time and the last known write time, up to a maximum number of hours configured for the collector. Continuous collection resumes only after the previous data has been recovered. Note: The
default recovery time is 0 hours. |
Throttle (Milliseconds) | Frequency of Wonderware data polling. To minimize the load on the Wonderware Server, the
configurable throttling option is provided by the Wonderware
Collector. By default, the Wonderware Collector tries to query
the tag data every 100 milliseconds based on the collection
interval time. You can change this value to any time between 100
milliseconds to 16 hours. Note: If
Throttle field is blank, enter
the required minimum value of 100 milliseconds.
|