Have You Seen Proficy Historian Lately?Click here to check out all the new features in the latest version.
Supercharge your GE solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Learn more about the Proficy 2023 releases, by signing up for one of our upcoming events.
If the Database menu
does not appear automatically:
Wait for approximately 90 seconds for the
connection timeout to occur.
After the 90-second timeout, the
Data Link Properties window
appears. Although it may appear as if Crystal
Reports has stopped working or is frozen before
the timeout occurs, this functionality is as
expected.
In the Data Source field, enter the Amazon Network Load Balancer (NLB) DNS.
Tip: To find the NLB DNS:
Access the EKS cluster on which you have deployed Proficy Historian for AWS.
Access the EC2 instance.
In the navigation pane, under Load Balancing, select Load Balancers.
Select the load balancer for which you want to find the DNS.
In the Description section, copy the DNS name.
Select OK.
Skip the next step.
If the Database menu
appears automatically:
Select Database > Set Location.
The Set Location
window appears.
Select Set
Location.
The Data Explorer
window appears.
Select a source, and then select
Set.
Select Done.
Results
The Historian server is connected with
Crystal Reports.