Known Issues and Limitations
The following issues have been identified in CIMPLICITY v2024:
Description | Tracking ID |
---|---|
Screen in CimEdit from the CIMPLICITY Workbench will not open if the project is placed in a directory with special names. For example, C:\MyProject_Automation\CIM_Ver2\. | SF-01120187 |
Unable to form logical links between primary and secondary servers in a redundant setup. | SF-01123046 |
String indexer for the CimClassList object does not work as expected. Working alternative is not documented well. | SF-00984050 |
Class dialogs have inconsistent Pre/Post Script selection behavior (Typed/Browsed). | SF-01077222 |
When only Proficy Authentication is enabled on the CIMPLICITY node, the login dialog appears and then disappears on a Webspace session, preventing login to the session. If mixed mode is enabled, the login dialog on the client appears correctly. | NA |
The following limitation has been identified in CIMPLICITY 2024:
Description | Tracking ID |
---|---|
The Redundant Configuration Update feature is not supported when opening a remote project over a UNC path. | NA |