Fixed Defects

The following issues have been fixed in CIMPLICITY v2024:

Description Tracking ID
Issue: Previously, PTDP_RP would stop after adding new derived points to the MB4SHM project, causing crash dump files to be generated.

Resolution: This issues has now been resolved. PTDP_RP no longer stops when there is an error in configuration for a derived point. A safety NULL check has been implemented to prevent crashes, informed by observations from dump analysis.

SF-01126986
Issue: Previously, attempting to install help while the project was in a running state was resulting in an error message.

Resolution: To prevent potential conflicts, help installation is now restricted when a project is running. Users will receive an error message if they attempt to install help while the project is active. The procedure in the help documentation is also updated accordingly. For more information on how to install local help, refer to https://www.ge.com/digital/documentation/cimplicity/version2024/oxy_ex-2/getting_started/topics/g_cimplicity_install_help_installer.html.

SF-01128506