RCO Function Blocks
Function blocks are the basic unit of execution in Routing Control Logic and output scripts.
A function block may be used in any type of script; however, some blocks have a specific purpose that limits their usefulness in certain types of modules. For example, a Select Decision
function block in an output module would serve no purpose. The decision has already been selected by the time the output module is selected. A Set Point
function block could be useful in either a logic or output module.
Routing Logic Modules (RLM) are used to select decisions. The list of available decisions is controlled by Routing Control Configuration. A logic module can only select or eliminate a decision in one specific site, it may not select or eliminate decisions in more then one site.
RCO supports the following types of function blocks:
BCO function blocks (available with Order Execution Mgt.). | |
Conditional function blocks. | |
Core function blocks. | |
Diagnostic function blocks. | |
Include file. | |
Output function blocks. | |
PRT function blocks. | |
Routing function blocks. | |
Range Source function blocks (available with Order Execution Mgt.). | |
RCO TADB function blocks (available with Order Execution Mgt.). |