Include File
Description
Includes the contents of the specified file into the generated script.
Parameters
This function block has the following parameters:
Parameter | Description |
Include File Name | The path of the file to be included. |
Include File Pseudo Code
#include"c:\proficy\includes\FuncsLib.txt"
Note: This function block works in the same way the #include"<file>" workin C/C++. This function block accepts a files that has only simple VB statements, and not the functions / sub-routines declaration. Since the entire contents of the file would be included with the Main function of the generated script.