Control site: Synchronous validation
Synchronous validation occurs during the control cycle to verify that a carrier has arrived at the stop position and allows the control site to stay in synchronization with the factory floor.
In the Tracker Config_UI, the following fields are configured to enable synchronous validation:
Dialog | Group Name | Field Name | Value |
Control Site | Execution Sequence | Verification Point | Point ID |
Verification Value | Boolean, integer or string |

1 | Control site for a split route. A routing decision must be made at this juncture. |
2 | A control cycle is in progress moving Monitor A to Region 4. |
3 | Monitor B has moved into the Split control site. |
4 | RCO waits for synchronous validation before allowing the control site to trigger. |