Ramp Setpoint
Ramp Setpoint enables users to add or subtract the standard and alternate values from the current value of a point, then perform a setpoint on the point using the modified value.
Configure the action as follows.

1 | Action type |
2 | Point ID |
3 | Offset |
4 | Allow edit |
5 | Alternate offset |
1 | Action type |
Select Ramp setpoint.
2 | Point ID |
Point on which a setpoint is performed.
- Offset values must be integers or real numbers.
- Point must be a Read/Write point.
![]() |
Opens the Select a Point browser. |
![]() |
Opens a Points Popup menu. |
3 | Offset |
Number added or subtracted from the point's value when a user
- Clicks the Up/Down arrows in the default box.
- Presses the Up/Down arrow keys.
4 | Allow edit |
Check to activate the runtime New Value edit field so a user can type a new offset value.
Checked or clear a user can use the Up/Down arrows in the Default and Alternate boxes to enter a new setpoint.
5 | Alternate offset |
Number added or subtracted from the point's value when a user:
- Clicks the Up/Down arrows in the Alternate box.
- Presses the Left/Right arrow keys.