Expression Setpoint
Expression Setpoint identifies a Point ID and an expression. When the procedure is invoked in CimView, the expression is evaluated using the trigger object to qualify variables in the expression. After the successful evaluation of the expression the value is downloaded to the Point ID.
Configure the action as follows.

1 | Action type |
2 | Point ID |
3 | Value |
4 | Confirmed |
1 | Action type |
Select Expression setpoint.
2 | Point ID |
Point that will be set when the action is triggered.
The:
- Value you select must be compatible with the point's type.
- Point must be a Read/Write point.
![]() |
Opens the Select a Point browser. |
![]() |
Opens a Points Popup menu. |
3 | Value |
Value the point will be set to when the action is triggered.
Valid entries are the same as valid entries for any field that accepts expressions, including:
- Point ID's.
- Variables.
- Absolute values.
- Expression operations.
4 | Confirmed |
(Optional) Runtime confirmation.
Checked | Requires confirmation. A message box will display before the action occurs requesting confirmation to proceed. |
Clear | Does not require confirmation. |
Default | Clear |