Known Issues in CIMPLICITY 2022

The following issues have been identified in CIMPLICITY v2022.

DE160167

Issue: To save the performer comments of an alarm on a CIMPLICITY client machine, you must upgrade the client to version 2022.

DE155485

Issue: When adding additional custom control from an assembly that controls have already been added from, the properties and methods for the additional controls are not included in the interface to the control.

Workaround: Change either IncludeBaseMembers or IncludeNewMembers flag to true based on your requirement. You must modify the flag in the GEIP.Orion.ComponentBuilder.config file located at <installation_location>\Proficy\Proficy CIMPLICITY\exe.

Issue: When IncludeNewControls flag is false, any new control that is added may appear on the UI, but it would not be functional.

Workaround: If you want to add a new control, you must ensure that IncludeNewControls flag is set to true in the GEIP.Orion.ComponentBuilder.config file located at <installation_location>\Proficy\Proficy CIMPLICITY\exe.