Fixed Defects in CIMPLICITY 2022

The following issue has been identified in CIMPLICITY v2022.

DE138491

Issue: Previously, if a screen was referenced in two locations, the screen path of the second screen was not displayed correctly in the navigation bar.

Resolution: This issue is now resolved. Now, when a screen is referenced in two locations, the screen paths are displayed correctly in the navigation bar.

US493575

Issue: Previously, when you downloaded a hardware configuration in PPS, the communication between CIMPLICITY and the PLC was lost, and the point values were not updated.

Resolution: This issue is not resolved. The points are now updated from the PLC, as expected.

US493573

Issue: Previously, when you shut down a PDS Port the device points created in other PDS ports would also become unavailable.

Resolution: This issue is resolved. When you shut down a PDS port the points of other PDS ports are not affected.