Variable Assign
Variable Assign assigns a Variable ID to a value or Point ID.
Configure the action as follows.
![](../common/../images/VDialogProcInfoVariableAssign.png)
Field | Description | ||
---|---|---|---|
1 | Action type | Select Variable assign. | |
2 | Variable ID | Variable on which the assignment is performed. | |
![]() |
?? | ||
![]() |
?? | ||
Specify either 3A or 3B. | |||
3A | Variable value | Text value that is not evaluated but is literally substituted for the Variable ID. The value specification can include, but is not limited to, a point ID, an expression that includes point ID's or absolute values. Important: If you enter a Variable value a user will not be able to change the value during runtime. | |
![]() |
?? | ||
![]() |
?? | ||
3B | Prompt for value | (Optional) When checked and the action is triggered during runtime, a Variable Assignment dialog box will open in which a user can enter a new value. Important: This feature will not work if the Variable value field has been filled in. |