What's New in CIMPLICITY 11.1
The HMI/SCADA CIMPLICITY v11.1 release includes the following new features and enhancements.
- Support for anti-alias
appearance optimization
The Text rendering section is introduced in the Compatibility tab of Global Configuration. It includes the following radio buttons:
- Non-anti-aliased: Anti-aliasing is not applied. Selecting this option is similar to de-selecting the anti-alias fontcheckbox in the previous versions.
- Anti-alias (speed optimized): Anti-aliasing is applied but it is speed optimized. Select this option for better performance. Selecting this option is similar to selecting the anti-alias fontcheckbox in the previous versions. This option is selected by default.
- Anti-alias (appearance optimized): Anti-aliasingis applied, and it is appearance optimized. Select this option for better font clarity than the Anti-alias (speed optimized) option.
- Support to include description for an
object in CimEdit
A Description text box is added to the General tab of the Properties screen of CimEdit. This enables you to add a description for an object. You can view the saved description in the Properties screen of CimEdit or CimView.
Note: For a linked object, the description of the source object is displayed in the Source Description section of the Link Container tab of the Properties screen. You can add a description for the linked object in the Description text box of the General tab.
- Enhanced the .Net Components
Feature
Previously, the newly added members/controls or members would not work as expected if there was a Dispatch ID mismatch. This issue has now been resolved. Whenever a new member or control is added, it is mapped to the next available ID.
Also, you can now modify the following properties as per your requirement in the GEIP.Orion.ComponentBuilder.config file located at <installation_location >\Proficy\Proficy CIMPLICITY\exe
-
Property Default Values Values IncludeBaseMembers <IncludeBaseMembers>false</IncludeBaseMembers> The base members are not included to object properties in CimEdit.
Set to True if you want to include base members to object properties in CimEdit.
IncludeNewMembers <IncludeNewMembers>false</IncludeNewMembers> When you upgrade .Net components version the, the new members introduced in the version, will not appear in object properties in CimEdit.
Set to True if you want to include newly introduced members to object properties in CimEdit.
IncludeNewControls <IncludeNewControls>true</IncludeNewControls> When you upgrade .Net components version the, the new controls introduced in the version, will appear in the .Net Component Browser in CimEdit.
Set to False if you do not want to include the newly introduced controls to the .Net Component Browser in CimEdit.
- Improved screen caching
algorithm
Previously, when you opened a screen or when there was a screen overlay, the cache logic searched for a screen that matched the screen name and project of the current screen.
Now, a global parameter GSM_CACHE_USE_VARS is introduced to improve the screen caching algorithm. When the value of GSM_CACHE_USE_VARS is set to Y, the cache logic searches for a screen with the same screen name, project, and initial variables. The default value of the parameter is N.
When the value of the parameter is N or if the parameter does not exist, the cache logic searches for a screen with the same screen name and project.
- Enhanced Logging Features
The logging feature if EM_LOG is now enhanced, for every run script action_type, a corresponding run script done, or run script abort, or run script error action_type would be logged. This enables you to know the status and time of an action.
Introduced PTMRP_CALOG_EU_VALUES to enable you to log the EU values in the point_val and point_prevval fields of CA_LOG.
- Introduced CIMPLICITY HMI Webspace
Plug-In
The CIMPLICITY HMI Webspace Plug-In is introduced to enable users to access CIMPLICITY CimView screens from Operations Hub. It can be integrated with other Operations Hub widgets for better consolidation and visualization of data. This provides the users an end-to-end solution for better data analysis, visualization, and monitoring.
In CIMPLICITY Options, the Webspace tab has been modified to include options to configure the servers. These configurations allow you to use Operations Hub authentication to access CimView screens from Operations Hub.
To enable seamless integration of the products some of the default ports have been modified. Also, you must open the firewall for some of the ports.
Service Default Port Number Firewall must be opened? NGINX 9443 Yes Webspace Application Publishing Service 491 Yes SCADA Web Configuration, REST 4955 No OPC UA browse service, REST 4956 No Webspace session Manager, REST 4957 No Webspace Session Manager, CimView socket 4958 Yes(*) Webspace Application Publishing Service 491 Yes Watch the following videos for demos on CIMPLICITY HMI Webspace Plug-in Setup:
- Introduced Buffer Data for Redundant
Failover Option
Buffer Data for Redundant Failover check box in introduced in Point Device Properties to enable PTMRP to buffer the data from OPC DA and UA in case of a failover. When you select Buffer data for redundant failover check box in Point Device Properties the data changes are buffered to avoid any data loss during the switch over. When the secondary server starts working, the relevant Alarms and Events can be generated based on the buffered data.
- Enhanced Point Configuration
Feature
PTMDP_DO_OVERRIDE_EXPR_RESULT_ALWAYS parameter is introduced to ensure that an equation with an override point is updated when the values of the source points are modified.
Introduced Log Only Option
The Change Approval feature is enhanced to include Log Only option. It enables you to log point changes into CA_LOG without any digital signature from users or services.
- Support to Use the Certificate of
External Certificate
Authority
Introduced new batch files Generate_CSR.bat and process_server_cert.bat that enable you to generate the Certificate Signing Request, and then process the SSL certificate received from external authority.
- Enhanced Cabling Redundancy
Feature
Introduced SOCKET_CONNECT_TIMEOUT to enable you to prevent the Windows Firewall from creating a failure mode. You must add this parameter to cimhosts.txt file. The optimal value may differ from system to system. However, the recommended range of values is >=2 seconds and <=5 seconds.
- Validated tracker configuration limits for
large region location counts
The maximum number of regions supported, depends on the PRT_DC process memory. If the memory utilized exceeds 4 gb, the following error appears in the status log: 'Not enough memory resources are available to process this command.'
The maximum number of available locations that are allowed in the region is 32767. The maximum number of items that can reside at a single region location is 32767. The maximum items per project should not exceed 33554429.
- Microsoft Access is no longer supported by CIMPLICITY.
- Portal is at its end of life, and its integration with CIMPLICITY is no longer supported. Contact your sales representative for alternate solutions.