System Requirements and Compatibility
Hardware Requirements
CIMPLICITY v11.1 requires, at a minimum, the following hardware specifications. GE Digital recommends testing your particular system to determine if your performance needs require hardware beyond the base system recommendations.
Hardware | Requirements |
---|---|
Microprocessor | Intel Core 2 Duo 3.0 GHz |
RAM | 4 GB |
Hard disk | 40 GB |
Ports |
|
Monitor |
|
Supported Operating Systems and Versions
CIMPLICITY v11.1 runs on any of the following operating systems, provided that specified revisions and service packs are included.
-
Microsoft® Windows® 10 (32-bit or 64-bit), Professional, Enterprise & Ultimate Editions
-
Microsoft® Windows® 8.1 (32-bit or 64-bit), Professional, Enterprise & Ultimate Editions
-
Microsoft® Windows® Server 2019
-
Microsoft® Windows® Server 2019 Cluster
-
Microsoft® Windows® Server 2016
-
Microsoft® Windows® Server 2016 Cluster
-
Microsoft® Windows® Server 2012 R2
-
Microsoft® Windows® 10 IoT Enterprise (LTSB) (Only full blown IoT version is supported. Not the core & mobile versions)
.NET Installation
NET 3.5 SP1 is required for the CIMPLICITY installer.
Supported External Software Versions
CIMPLICITY v11.1 is compatible with the following external software.
External Software | Supported Version |
---|---|
Microsoft Office | 2016 and 2019 |
Microsoft SQL Server |
2014, 2016, 2017, and 2019 Important: SQL Server 2008 can be installed but is no longer supported.
Note: CIMPLICITY has been validated to work with Database configurations using SQL 2016 AlwaysOn with the exception of the Tracker Attribute Database (TADB) functionality.
|
SQL Express | 2014, 2016, 2017, and 2019 |
Oracle |
18c and 19c Note:Both the client and server should be running same version of Oracle. |
Microsoft Visual Studio | 2017 |
Flexera Software - Install Shield | 2018 |
Sequent - Alarm Cast | 10.02.01 |
Supported GE Software Versions
CIMPLICITY v11.1 is compatible with the following GE software.
GE Software | Supported Version | Install Before or After CIMPLICITY |
---|---|---|
Alarm Cast Administrator | 10.02.01 | After |
Change Management | 9.5 | Before |
Common Licensing | Latest version | With CIMPLICITY |
Driver Server | Latest version | Either |
Global Discovery Server | 2.2 | After |
Historian (full version) | 9.0 and 8.1 Note: Logging array points to Historian is supported from version 7.0 onwards. |
Either |
IGS OPC Server | Latest version | Either |
Machine Edition | 9.5 and 9.0 | Either |
Plant Apps | 8.2 and 8.1 | Either |
Portal | 3.5 SP5 | Either |
Proficy Driver Server (PDS) * | Latest version | With CIMPLICITY |
OPSHUB | 2.0 SIM 4 | After |
Webspace | 6.0.3 | After |
Starting CIMPLICITY 11.1 , the Proficy Driver Server will not be installed with CIMPLICITY installation.
To install Proficy Driver Server, navigate to the CIMPLICITY Install Media located at Setups\Proficy Driver Server\setup.exe. Before you install Proficy Driver Server, you must install .NET Framework 3.5 through your Windows options.
-
If you are already using the Proficy Driver Server in your CIMPLICITY projects, it will continue to work as expected. Existing PDS is not uninstalled when you uninstall CIMPLICITY and upgrade to 11.1.
-
The Driver Server protocol may be enabled in Project Properties even when Proficy Driver Server is not installed.
Compatibility Requirements
Note the following as they apply to your installation:
Element | Requirement |
---|---|
Network Communication I/O |
Allen-Bradley Ethernet Driver Note the following:
Windows 2019 Windows 8.1 Windows 10 Server2012R2 Server 2016 Windows 10 IoT, LTSB Note: Depending on the OS, some RSLINX OEM features may not be supported. Refer to the RSLINX documentation for further information.
|
Genius PCI |
If you are using Genius PCI communications you need:
Note: Genius PCI is only supported on 32-bit Windows 7 and Windows 10 systems.
|
Reflective Memory |
If you are using reflective memory, the card requirements are:
Note: You can install up to two reflective memory cards, but not all computers support two cards due to hardware or BIOS-specific limitations. The Reflective Memory driver is only supported on Windows 7 and is no longer packaged with CIMPLICITY. However, the package is available from Abaco, who is also the vendor for the reflective memory cards.
You must install the following package: RFM2G Windows 7/XP/Vista/Server 2008/Server 2003/32/64-bit PCIE/PCI/PMC Driver for X86 R08.01. |
DDE Communications |
The DDE communications interface runs in the service session only. The DDE server must be able to run from the service session. |
Browsers |
The following browsers are supported for Webspace with CIMPLICITY.
The following browsers are supported with the SCADA Web Configuration:
|